SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
In the case that an error occurs during any Rx operation, the UDMA will stop processing the TR at that point and will return an appropriate error code in the Transfer Response message as specified in the TI DMA Architecture specification. The PAUSE_ON_ERR bit in the RCHAN UDMA_RCFG_j registers controls whether or not the DMA will pause operation on that channel if an error or exception occurs. If the PAUSE_ON_ERR bit is set to 1 the channel will be paused so that the host can optionally read the channel state to determine where in the transfer the channel execution was. If the PAUSE_ON_ERR bit is 0 the DMA will flush the current Transfer Request record for channels in pass by value mode and will flush the current Transfer Request Descriptor for channels in pass by reference mode.