SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The following interrupts are generated by the NF module (see Table 6-176):
| Interrupt | Description |
|---|---|
| NF_FRAME_DONE | Frame processing complete. |
| NF_SL2_READ_ERROR | Set whenever there is an error response on VBUSM read command request for any input channel. |
| NF_SL2_WRITE_ERROR | Set whenever there is an error response on VBUSM write command request for any output channel. |
All interrupts are single pulse event signals that are mapped to the VPAC level interrupt aggregation logic.