SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
This is the offset of the destination address from the initial destination address for the first access of the outer loop. This will be added to the destination address from the loop before. This is a signed value so that the destination address can be both above and below the initial destination address.