SPRUJ28F November 2021 – August 2025 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The R5F core generates several events as part of event bus that can be monitored by the PMU for debugging. The memory ECC related events from the event bus are exported to ESM for monitoring.
There are four ECC interrupts to the ESM that aggregate different categories of ECC events – CPU0 single error, CPU0 multi error, CPU1 single error, and CPU1 multi error events. Each ECC event has a 2-bit event bus counter associated with it. Everytime an event occurs, the counter is incremented by 1 till it reaches the max value of 3. The interrupt is asserted if the bus counter of any event associated with the interrupt is non-zero.
Each event bus counter has a MMR decrement control to decrement the counter by 1. So, for example, if a counter value is 2, the MMR to decrement the counter would need to be written 2 times to decrement the counter to 0. The reason decrement control has been added instead of clear control is if a new error occurs between the time the status register is read and the clear MMR is written, the new error would be lost. Write-to-decrement ensures that this does not happen.
When all event bus counters of an associated interrupt are zero, the interrupt is cleared. It takes three clock cycles for the event bus counter to be decremented once the write to the decrement control MMR presents itself at the R5FSS boundary.
Since each of the four ECC interrupts have single bit control to set the interrupt but multiple bits for clearing it, note that once an interrupt is set using the R5FSS_EVNT_BUS_ESM_SET register, it can be cleared by setting all the bits of the R5FSS_EVNT_BUS_ESM_CLR register that correspond to that particular interrupt. For example, if bit [0] of the R5FSS_EVNT_BUS_ESM_SET register is set, it can be cleared by setting bits [7-0] of the R5FSS_EVNT_BUS_ESM_CLR register to clear the interrupt.
The R5F core event bus only signals event when it is enabled. Non-invasive or invasive debug mode needs to be enabled to enable the PMU counters.
The export of the events to the event bus can be enabled by setting the X bit in the Performance Monitor Control Register of the R5F core. For more details, refer to Arm R5 TRM.
| Event Bus Bit # | Description | Associated Status Register |
|---|---|---|
| 22 | Instruction cache tag RAM parity or correctable ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[1:0] EVNT_BUS0 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[1:0] EVNT_BUS0 |
| 23 | Instruction cache data RAM parity or correctable ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[3:2] EVNT_BUS1 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[3:2] EVNT_BUS1 |
| 24 | Data cache tag or dirty RAM parity error or correctable ECC error, from data-side or ACP | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[5:4] EVNT_BUS2 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[5:4] EVNT_BUS2 |
| 25 | Data cache data RAM parity error or correctable ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[7:6] EVNT_BUS3 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[7:6] EVNT_BUS3 |
| 40 | ATCM single-bit ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[9:8] EVNT_BUS4 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[9:8] EVNT_BUS4 |
| 41 | B0TCM single-bit ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[11:10] EVNT_BUS5 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[11:10] EVNT_BUS5 |
| 42 | B1TCM single-bit ECC error | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[13:12] EVNT_BUS6 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[13:12] EVNT_BUS6 |
| 43 | TCM correctable ECC error reported by load/store unit | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[15:14] EVNT_BUS7 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[15:14] EVNT_BUS7 |
| 44 | TCM correctable ECC error reported by prefetch unit | R5FSS_CPU0_EVNT_BUS_SB_ERR_CNT_STATUS[17:16] EVNT_BUS8 R5FSS_CPU1_EVNT_BUS_SB_ERR_CNT_STATUS[17:16] EVNT_BUS8 |
| Event Bus Bit # | Description | Associated Status Register |
|---|---|---|
| 26 | TCM fatal ECC error reported from the prefetch unit | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[1:0] EVNT_BUS0 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[1:0] EVNT_BUS0 |
| 27 | TCM fatal ECC error reported from the load/store unit | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[3:2] EVNT_BUS1 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[3:2] EVNT_BUS1 |
| 33 | Data cache data RAM fatal ECC error | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[5:4] EVNT_BUS2 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[5:4] EVNT_BUS2 |
| 34 | Data caches tag/dirty RAM fatal ECC error, from data-side or ACP | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[7:6] EVNT_BUS3 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[7:6] EVNT_BUS3 |
| 37 | ATCM multi-bit ECC error | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[9:8] EVNT_BUS4 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[9:8] EVNT_BUS4 |
| 38 | B0TCM multi-bit ECC error | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[11:10] EVNT_BUS5 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[11:10] EVNT_BUS5 |
| 39 | B1TCM multi-bit ECC error | R5FSS_CPU0_EVNT_BUS_MB_ERR_CNT_STATUS[13:12] EVNT_BUS6 R5FSS_CPU1_EVNT_BUS_MB_ERR_CNT_STATUS[13:12] EVNT_BUS6 |