SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
| Bits | Name | Description |
|---|---|---|
| 31:27 | Packet Type | Host Packet Descriptor Type = 0xa |
| 26 | Mode | 0= Normal, 1=TILED |
| 25 | Direction | Inbound = 0, Outbound = 1 |
| 24:16 | Channel | Channel for which this descriptor describes |
| 15 | Reserved | Reserved for future use |
| 11:9 | Priority | Only Bit 9 and Bit 11 are used to set the priority. Bit 10 is ignored. Highest = 0, Lowest = 3 By default, hardware assigns priority = 3. This priority level is used in the arbitration between the masters (for DDR access). See Section 11.4.8.8.1.4.5, Priority, for more details. |
| 8:0 | Next Channel | Next Channel to execute on a line or the channel to use in the generated write descriptor. |