SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
When a source-synchronized channel is disabled during a transfer, the current hardware request (element/packet/frame/block) service completes and the channel DMA4_CCRi[9] RD_ACTIVE bit is set to 0, which means the channel is not active on the read port. The remaining data in the corresponding disabled channel FIFO is drained onto the write port and transferred to the programmed destination as in normal transfer.
At the end of the draining the DMA4_CCRi[10] WR_ACTIVE bit is set to 0 (channel is no longer active on the write port) and if the DMA4_CICRi[12] DRAIN_END_IE is set to 1, the DMA4_CSRi[12] DRAIN_END status bit is updated and an interrupt is generated.
Once a channel is disabled during a transfer, it must wait for the DMA4_CCRi[9] RD_ACTIVE and DMA4_CCRi[10] WR_ACTIVE bits to become 0 before being reenabled for a new transfer. The FIFO drain for a channel occurs only in the following cases:
For a self-linked or chain-linked channel, the user must disable the DMA4_CLNK_CTRLi[15] ENABLE_LINK bit before disabling the channel.
In all other cases, the channel undergoes an abort.