SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P
The DSP_EDMA traffics initiated on the DSP EDMA master port can be optionally routed through the DSP_MMU1 on the EDMA address path. This is controlled in two levels :
For the DSP_MMU1 to operate, SW should enable it both at the DSP_SYSTEM global level and DSP_MMU1 local register level.
When enabling the DSP_MMU1, software must take care that no transactions are in flight through that MMU. This is typically handled by disabling any EDMA transactions prior to enabling the MMU. Note that the local enable bit inside the DSP_MMU1 must be configured as normal (refer to the Chapter 22,Memory Management Units.)
For more information on the MFENCE operation, refer to the section, C66x CPU Instruction Set of the TMS320C66x DSP CPU and Instruction Set ).
In addition, the DSP_MMU1 traffic can be aborted in case of a lockup via the DSP_SYS_MMU_CONFIG [12] MMU1_ABORT bit. In other words, this bit can be used to clear a hang condition that may occur if the DSP_MMU1 encounters a page fault that cannot be serviced.
For more information on device DSP_MMU1 functionality and settings, refer to the Section 22.3, MMU Functional Description and the Section 22.5, MMU Register Manual, in the chapter, Memory Management Units, respectively.