SPRADO8 March 2025 AM62L
The baseline drive impedance and ODT settings for memory (DDR4/LPDDR4) derived from the signal integrity (SI) simulations performed on the EVM.
The recommendation is to perform simulation for the custom design as the configuration values can differ.
Refer to the FAQs:
[FAQ] Using DDR IBIS Models for AM64x, AM62x, AM62Ax, AM62Px
The FAQs are generic and can also be used for AM62Lx processor family.
To get an overview of the board extraction, simulation, and analysis methodologies for high speed LPDDR4 interface, see LPDDR4 Board Design Simulations chapter of the AM62x DDR Board Design and Layout Guidelines application note.
The drive strength is adjustable using the DDR Register Configuration Tool on SysConfig.
For more information, refer to the FAQs:
[FAQ] AM62A3-Q1: AM62A3-Q1 PDN Power SI SIMULATION Questions
The FAQs are generic and can also be used for the AM62Lx processor family.