SPRADO8 March 2025 AM62L
The following (UART, MCAN, MCSPI, MCASP, I2C) peripherals implements IOSET. Make sure the usage of the correct IOSET in the custom design.
Timing closure is based on the IOSETs.
Verify the IO supply for IO group that is referenced by the IOs (fixed or dual-voltage) of the connected processor peripheral and the IO voltage level of the attached device are compatible. The recommendation is to connect the IO supply of the attached device and the IO supply for IO group referenced by the connected processor peripheral IOs are connected to the same supply source.
For the number of MCAN instances supported, see the processor-specific data sheet. The MCAN interface to the processor includes external MCAN transceiver.
When an external transceiver is used, match the external interface signal IO levels with the dual-voltage IO supply for IO group voltage level.
Provide the required terminations for the MCAN transceiver.
The recommendation is to provision for series resistors on the interface signals (close to source) for isolation or debug.