SPRADO8 March 2025 AM62L
Refer to the note regarding shared IO pins in the Device Comparison section of the processor-specific data sheet. IOSETs are a grouping of signals specific to an interface that are timed as a set including the supply rails voltage level. The IOSETs make sure that the same IO supply for IO group is used for the signal pairs. IOSETs are enforced by the SysConfig tool. The processor is timing closed using IOSETs. Any interface that has IOSETs is recommended to select all interface signals from the same IOSET. Some interface signals can be shared over multiple IOSETs. The valid pin combinations are detailed in the SysConfig-PinMux tool. Take note of possible IO supply for IO group mismatch between the IOs used for a specific interface based on the use case.
Refer to the FAQ for information on Voltage conflict and IOSET: [FAQ] AM625 / AM623 / AM62A / AM62P / AM62D-Q1 / AM64x / AM243x Design Recommendations / Custom board hardware design - Queries related to SysConfig-PinMux IOSET and Voltage Conflict
The FAQ is generic and can also be used for AM62Lx processor family.