SPRADO8 March 2025 AM62L
LFOSC0 has limited use cases and is optional. Based on the use case, select a 32.768kHz crystal as the clock source or a 1.8V LVCMOS square-wave digital clock source.
For more information, refer to the FAQ: [FAQ] AM625: LFOSC usage in the device.
The FAQ is generic and can also be used for AM62Lx processor family.
Place all discrete components used to implement the oscillator circuit as close as possible to the LFOSC0_XI and LFOSC0_XO pins. For the crystal, the load capacitance selected is required to be in the range recommended in the LFOSC0 Crystal Electrical Characteristics table of the processor-specific data sheet.
If LFOSC0_XI / LFOSC0_XO is not used, then the recommendation is to connect the XI directly to the VSS and to leave the XO unconnected.
For more information on connecting the unused LFOSC0, see the LFOSC0 Not Used section of the processor-specific data sheet.