SPRADO8 March 2025 AM62L
Connect USBn_DM and USBn_DP signals directly from the processor to the USB hub upstream port. The hub then distributes USBn signals to the downstream ports as needed. As each hub has different implementation requirements, follow the hub manufacturer recommendations.
For more information on USB2.0 interface, to the below FAQ: [FAQ] AM625 / AM623 / AM625SIP / AM625-Q1 / AM620-Q1 Custom board hardware design – USB2.0 interface
The FAQ is generic and can also be used for the AM62Lx processor family.