SPRADO8 March 2025 AM62L
Verify the IO supply for IO group that is referenced by the IOs (fixed or dual-voltage) of the connected processor peripheral and the IO voltage level of the attached device are compatible. The recommendation is to connect the IO supply of the attached device and the IO supply for IO group referenced by the connected processor peripheral IOs are connected to the same supply source.
Refer to the data sheet for the supported GPMC interface configuration.
Non Muxed-Nor interface is not supported due to the number of address lines pinned out. The description for GPMC0_A0-A6 is the IP functional description (not the pin function description).