Note: LVCMOS IOs can be referenced to fixed 1.8V or
fixed 1.8V/3.3V IO supply for IO groups. Verify the IO level compatibility with the
attached device. The recommendation is to power the processor IO supply for IO group
and the attached device IO supply from the same power source. The board designer
must make sure the design does not apply a potential that is greater than the values
defined in the Absolute Maximum Ratings table.
Verify the IO supply for IO group that is referenced by the IOs (fixed or dual-voltage) of the connected processor peripheral and the IO voltage level of the attached device are compatible. The recommendation is to connect the IO supply of the attached device and the IO supply for IO group referenced by the connected processor peripheral IOs are connected to the same supply source.
Refer to the FAQ: [FAQ] AM625 / AM623 / AM62A / AM62P /
AM62D-Q1 / AM64x / AM243x Design Recommendations / Custom board hardware
design - Data sheet Pin Attributes and Pin connectivity related
queries
The FAQ is generic and can also be used for the
AM62Lx processor family.