SPRADO8 March 2025 AM62L
For peripherals naming and instances, the processor-specific TRM tends to be generic and the processor-specific data sheet is specific.
In the data sheet, a suffix number is assigned, even when there is a single peripheral instance. Documents that reference the peripheral name do not need to change from processor to processor.
The suffix starts with 0. For the common platform Ethernet switch 3-port gigabit (CPSW3G) port names, port 0 is the internal (communications port programming interface (CPPI) host) port of the switch.