SPRADO8 March 2025 AM62L
The recommendation is to add required design notes for the processor peripherals. For example, USB2.0 interface, Ethernet interface, Display interface (DSI0), eMMC, OSPI, SD, and other available processor peripherals). Notes added can include board boot mode configurations, placement of series and parallel resistors, placement of decoupling and bulk capacitors.
Consider adding the required or applicable design notes to the processor attached devices and onboard devices.
Mark all differential signals, critical signals and specify the target impedance (as required). See the following examples:
See the following FAQs:
[FAQ] AM625: PCB Pattern Recommendations for Specific Peripherals
[FAQ] AM625: MMC0 PCB Connectivity Requirements
AM6442: PCB layout guidelines for MMCSD0(eMMC) and MMCSD1(SD card)
The FAQs are generic and can also be used for AM62Lx processor family.