SPRADO8 March 2025 AM62L
Once the schematics design is completed following the design guidelines provided in the user's guide and referring to the EVM schematics and other available collaterals, the board designer can do a self-review using the checklist provided at the end of each design guidelines section.
Example:
Processor Core and Peripheral Core Power Supply Checklist
General Board Bring-up and Debug Checklist
The FAQ lists the collaterals and steps that can be followed for performing self-review of custom board schematics:
The FAQ lists common errors observed while reviewing customer schematics. The recommendation is to read the list and make the required updates:
The FAQ is generic and can also be used for AM62Lx processor family.