SPRADO8 March 2025 AM62L
Series resistor on the clock output near to the processor clock output pin is recommended to resolve issues with signal distortion at the source of the clock since the clock output is also used for retiming. For MMCx and OSPI, an unbonded pad is used (internal), so a series resistor is not a requirement. In some cases, a low value series resistor is added for signal integrity purpose. The recommendation is to have the series resistor as a place holder just in case for improving signal integrity.