SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
To trigger an application, follow these steps:
Program the update image in the corresponding slot:
For Overwrite mode:
App 0 update images must be flashed to scfg.flashCfg.flashLayout.secondaryAppSlots[0].
App 1 update images must be flashed to scfg.flashCfg.flashLayout.secondaryAppSlots[1].
For XIP mode:
App 0 update images must be flashed to the slot these have been linked for.
Call HapiSbSetUpdateImageAddress( 0 )
Call HapiSbSetId( 3 )
Reset the device
When the system is being provisioned for the first time, the target image can be programmed directly to the slot in which it will be executed.
Application images must be signed with the key that corresponds to the App active key in the Key Ring.
Refer to the Secure Boot SDK example for instructions on how to create Application update images.