SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755P10 , CC2755R10
In general, Secure Boot compatible images must adhere to the following format:
Figure 11-6 Secure Boot Image Format. Note:
SB: Secure Boot Header
TLV: Type Length Value
Tools in the SDK are provided to create Secure Boot compatible images. Refer to the Secure Boot example in the SDK for detailed instructions.
To get more details about the image header and TLV fields, refer to MCUBoot Image Format.