SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
The fallback mechanism allows Secure Boot to boot the Secondary Secure Bootloader (if valid) if it is determined that the Application cannot be booted.
Alternatively, if Secure Boot is requested to boot a Secondary Secure Bootloader but it is determined that it cannot be booted, then Secure Boot will fallback to attempt to boot the Application (if valid).
By design, if application slots are undefined, Secure Boot will fallback to boot the Secondary Secure Bootloader (if valid) and will set the status as Invalid Configuration.