SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Every channel has an input that is used when the channel is configured in a capture action. The channel input can come from different sources, can be filtered, and goes through an edge detection logic before triggering the channel capture. See Figure 12-3 detailing the input logic.
If the FAULT register is present, then enabling the FAULT logic uses channel 0 as the fault input. The CnCFG.INPUT field configures if the input comes from the IOC or Event logic. The channel filter can be configured to require up to CHFILT.LOAD +1 consecutive input samples before the input is propagated to the edge detection logic. This can typically be used to avoid capturing on glitches. After the channel filter, the input goes into the edge detection logic. This is configured in the CnCFG.EDGE field.
The different components of the capture data path are clocked as follows: