SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
Peripheries are by default mapped in the NSC marked region 0x4000 0000 - 0x4FFF FFFF. Each periphery has a gasket that can move it into the 0x5000 0000 0x5FFF FFFF range which is marked NS. This happens when a control signal is sent to the gasket from the TCM. The gaskets shall only be configured at boot. Run-time reconfiguration outside of TI delivered code is not supported and may lead to malfunctions. The new address is given by the old address + 0x1000 0000.
An access to a region where the periphery is NOT mapped will not result in a BusFault, instead you will read zero/ignored write.