SWCU195A December 2024 – May 2025 CC2744R7-Q1 , CC2745P10-Q1 , CC2745R10-Q1 , CC2745R7-Q1 , CC2755R10
There are two special modes that can be entered where the flash is completely isolated from the rest of the design, and no reads, writes, or erasures can be performed. These modes are designed not to allow the contents of flash to be read out or modified in any way. These modes are forbidden if either the SCFG or CCFG forbids the allowToolsClientMode permission. As described in Section 10.1, the most secure configuration is to disable these modes. However, to enable either mode, both the SCFG and CCFG must have the allowToolsclientMode permission set to enabled.