SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The ECAP module represents one complete capture channel, which has the following independent key resources:
Multiple identical ECAP modules can be contained in a system as shown in Figure 12-2197. For actual number of the ECAP modules integrated in the device, refer to the ECAP Integration. The letter x within a signal or module name is used to indicate a generic ECAP instance on a device. For example, output interrupt request, ECAP1INT belongs to ECAP1, ECAP2INT belongs to ECAP2, and so forth.
Figure 12-2197 Multiple ECAP Modules