SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The TR is able to select up to 2 of 3 trigger sources for a given TR. The events can come from the dedicated local event on the BCDMA itself or from two assigned global events that come from the PSI-L interface on the BCDMA. The trigger counters are always enabled so that events can be received prior to the TR getting loaded. The trigger counters are only decremented when the trigger is active and the TR has scheduled the first transfer of the transaction.