SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The glitch filter is a block which is used to reject pulses smaller than width, defined in the ICSSG_PWM0[7-0] PWMm_DEBOUNCE_VALUE. For example , if bit field [7-0] PWM0_DEBOUNCE_VALUE is set to 10h, a pulse which is less than 16 x ICSSG_CORE_CLK clock cycles will be filtered.