The following lists changes that must
be considered compared to previous generation CSI_TX_IF:
- YUV420 is not supported, YUV420
configuration registers/bitfields are not used
- Word count must be programmed in
the CSI_TX_IF, not in the TX Core.
- CSI_TX_IF compatibility mode must
be used in Stream0 when retransmitting from CSI_RX_IF