SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The sequence for using ADMA is shown in Figure 12-194.
(1) Create Descriptor table for ADMA in the system memory.
(2) Set the Descriptor address for ADMA in the MMCSD0_ADMA_SYS_ADDRESS register.
(3) Set the value corresponding to the executed data byte length of one block in the MMCSD0_BLOCK_SIZE register.
(4) Set the value corresponding to the executed data block count in the MMCSD0_BLOCK_COUNT register in accordance with Determination of Transfer Type.
(5) Set the argument value to the Argument register (MMCSD0_ARGUMENT1_LO and MMCSD0_ARGUMENT1_HI).
(6) Set the value to the MMCSD0_TRANSFER_MODE register. The Host Driver determines Multi/Single Block Select, Block Count Enable, Data Transfer Direction, Auto CMD12 Enable and DMA Enable in the MMCSD0_TRANSFER_MODE register. Multi/Single Block Select and Block Count Enable are determined according to Determination of Transfer Type. If response check is enabled (MMCSD0_TRANSFER_MODE[7] RESP_ERR_CHK_ENA = 1), set MMCSD0_TRANSFER_MODE[8] RESP_INTR_DIS bit to 1 and select Response Type R1/R5 (MMCSD0_TRANSFER_MODE[6] RESP_TYPE).
(7) Set the value to the MMCSD0_COMMAND register.
Note: When writing to the upper byte [3] of the MMCSD0_COMMAND register, the SD command is issued and DMA is started.
(8) If response check is enabled, go to stop (11) else wait for the Command Complete Interrupt (MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit).
(9) Write 1 to the MMCSD0_NORMAL_INTR_STS[0] CMD_COMPLETE bit to clear this bit.
(10) Read Response register (MMCSD0_RESPONSE_0 - MMCSD0_RESPONSE_7) and get necessary information of the issued command.
(11) Wait for the Transfer Complete Interrupt (MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE) and ADMA Error Interrupt (MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE).
(12) If MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit is set to 1, go to Step (13) else if MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE bit field is set to 1, go to Step (14).
(13) Write 1 to the MMCSD0_NORMAL_INTR_STS_ENA[1] XFER_COMPLETE bit to clear this bit.
(14) Write 1 to the MMCSD0_ADMA_ERR_STATUS[1-0] ADMA_ERR_STATE bit field to clear this bit.
(15) Abort ADMA operation. SD card operation should be stopped by issuing abort command. If necessary, the Host Driver checks MMCSD0_ADMA_ERR_STATUS register to detect why ADMA error is generated.
Note: Step (3) and Step (4) can be executed simultaneously. Step (6) and Step (7) can also be executed simultaneously.