SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
On each cycle, an arbiter built into the initiator side of each interface decides on which thread to transfer data in the next clock cycle. Both forward (from source threads) and reverse (from destination threads) direction transfers can occur across the same physical interface so the arbiter must ensure that sustained blocking of any thread can occur.
The decision about which thread to allow using the interface is based on the following factors:
No thread can be considered for inclusion in arbitration unless both data is available and credit exists in the destination endpoint. For each thread which can be considered in the current arbitration cycle, the arbiter should then pick the thread with the highest priority. Reverse transfers should be considered higher priority than forward transfers.