SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
This section provides the detailed description of the two instances of the motion adaptive merge.
Figure 7-32 shows the high level block diagram of the MA merge block
The MA block receives two inputs each of which can be up to 16 bits. As mentioned earlier, the ordering of the long and the short exposure cannot be changed and should be positioned as it’s depicted in the figure above. The MA block consists of 3 main sub-blocks, which are described in the following sub-sections.