SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
This section describes the teardown procedure for internal Tx channels within the PKTDMA. A Tx channel teardown is initiated by the host by writing the tx_teardown bit in the Tx Channel N Real-time Control Register (<TCHANRT[a]_TRT_CTL > [30] TX_TEARDOWN).
Once the host has written the tx_teardown bit, the PKTDMA will do the following:
Stops performing any additional descriptor fetches for the channel.
Completes any packets normally for which a pointer/descriptor/TR fetch has already been performed.
Sets the tdown bit on the EOP data phase of the last packet to be sent (if any traffic was pending when teardown was initiated) or sends a zero byte packet with the tdown, sop, and eop bits asserted. This signals the destination thread that all of the data has been sent.
Clears the channel enable in the Tx Channel N Global Configuration Register (<TCHANRT[a]_TRT_CTL> [31] TX_ENABLE).
Resets the channel state (including scoreboards, FIFOs, counters, statistics, etc.) to their after reset values.
Sets bit 31 of the Tx Flow Reverse Ring Occupancy register (<RINGRT[a]_RT_ROCC> [31] TDOWN_COMPLETE) to indicate that a teardown has completed.
If the current Tx reverse ring occupancy is 0, issues an Tx reverse ring completion up event which is then routed to an IA and can be further routed to any event consumer.
If the current TX Reverse ring occupancy is not 0 then a write to the doorbell with a negative value of the current occupancy will clear any remaining work but the forward ring pointer will remain the same. If the ring pointer needs to be reset then perform a write to any of the ring configuration registers.
The host may issue a teardown on any channel at any time, regardless of whether the channel is actively receiving a packet or not.
The Host can determine that a teardown is complete by using either of the following methods:
Periodically polling the teardown and enable bits for the channel
Waiting for an interrupt and observing the teardown complete bit is set in the channel’s default flow (first flow in channel) reverse occupancy register (<RINGRT[a]_RT_ROCC> [31] TDOWN_COMPLETE) for the channel.