SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
In start-bit mode, an extended bit is added before the MCSPI word to indicate whether the next MCSPI word must be handled as a command or as data. This feature is available only in controller mode. Start-bit mode cannot be used at the same time as turbo mode and/or force SPIEN_[n] mode. In this case, only one channel can be used; round-robin arbitration is not possible.
This mode is programmable per channel by setting the MCSPI_CHiCONF[23] SBE bit to 1. The polarity of the extended bit is programmable per channel. When the MCSPI_CHiCONF[24] SBPOL bit is set to 0, the MCSPI word must be handled as a command. When the MCSPI_CHiCONF[24] SBPOL bit is set to 1, the MCSPI word must be handled as data. Moreover, start-bit polarity can be changed dynamically during start-bit transfer without disabling the channel for reconfiguration; in this case, users must configure the MCSPI_CHiCONF[24] SBPOL bit before writing the MCSPI word to be transmitted to the TX register.