SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The DSI video operation requires the configuration of the VSG and TVG registers to match the panel configuration. The two video interface options will also require careful selection of the clock and registers to achieve error free video streaming.
The DSITX controller supports the mechanism for initial skew calibration for D-PHY data rates greater than 1.5 Gbps.
DPI Video Interface Operation
The time taken to output a frame on the PPI needs to match what is coming in on the DPI. This is best achieved by using the recommended clock ratio between the pixel and byte clocks. If this is the case, then the blanking and active data periods must be matched up. The DSI controller will match its frame timing to the incoming DPI VSYNC, if it is programmed to generate a frame of slightly less than the same size when the VFP blanking is considered.
The controller works by transitioning to LP during the last programmed line of VFP. It will then remain in LP until the start of the next frame. So, programming the controller to match the DPI, but with at least one fewer line of VFP should result in a reliable configuration.
Program the DSI vertical size registers as follows:
The timing should also be matched per line, therefore the blanking and active periods should match. DPI horizontal timing is measured in pixels, whereas the DSI controller uses bytes. If any of the DPI related interrupts are triggered, then this highlights that the FIFO depth and/or the vsync_delay settings require to be tuned to the current configuration. Simulating the core operation with the expected clocks is the best way to ensure the FIFO depth and vsync_delay is suitable.
The relationship therefore depends upon the pixel format, which could be 24, 18 or 16 bpp. Additionally, the PPI short packets and packet headers that are inserted by the controller must be accounted for. HSA should be reduced by 14 bytes to account for the HSS short packet (4 bytes), the long blanking packet header and footer (4 + 2 bytes) and the HSE short packet (4 bytes). HBP should be reduced by 12 to account for the header and footer on the blanking packet (6 bytes) plus the header on the active data packet (6 bytes). HFP should be reduced by 6 bytes to account for the long packet header and footer. Finally, for lines with no active data, the BLKLINE_PULSE_PCK is the total size minus 20 bytes (14 for HSA, 6 for the remaining blacking which is all combined into a single packet).
Program the DSI horizontal size registers as follows:
TVG Generator
The TVG oversees generating dummy data (to display something even if there is no video stream running). It is also able to ease verification or validation of the DSI without having a complete environment (application or verification test bench). The controller has a Test Video Generator that can be programmed to generate a set of test colour patterns based on the display panel that will be used. The panel parameters for horizontal and vertical resolution along with the frame rate and pixel colour depth need to be set based on the datasheet information for the panel.
Figure 12-527 presents TVG MODE patterns.
The TVG generates a data stream in the same format than the one specified for the normal functional video stream (as set in VSG register). The content of that flow is specified by registers. Those registers specify the following information: Image size: Number of bytes per line (see TVG_LINE_SIZE[14:0] register) and number of lines per frame (TVG_NBLINE[12:0]).
Image kind: Single color, vertical stripes or horizontal stripes (see TVG_MODE[1:0] register). Stripe width: Significant when a stripe mode is enabled. Possible values are 1, 2, 4, 8, 16, 32, 64 and 128 (see TVG_STRIPE_SIZE[2:0] register).
Pixel kind: 16 bits RGB, 18 bits RGB, 18 bits loosely RGB, 24 bits RGB, 30 bits RGB or 36 bits RGB (see VID_PIXEL_MODE[3:0] register).
Color one: Color used in single color mode or first color when in stripe mode. 12 bits per component R/G/B. For formats using fewer bits than 12, the least significant ones are the ones considered (see COL1_GREEN[11:0], COL1_RED[11:0], COL1_BLUE[11:0] registers).
Color two: Color two when in stripe mode. 12 bits per component R/G/B. For formats using fewer bits than 12, the least significant are the one considered. (see COL2_GREEN[11:0], COL2_RED[11:0], COL2_BLUE[11:0] registers). Start pulse and stop handshake (+ stop mode) (see TVG_CTL register).
An example of the sequence is as follows:
Note: The number of lines per frame and number of bytes per line. It is required that TVG settings on active area match VSG settings on active area. Any mismatch will create an error that is detected in the VSG and forces recovery mode in TVG, stopping test frame generation.