SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
After the first N virtIDs for DMA class usage, the remaining virtIDs up to the maximum allowed (as set in PVU_VIRTID_MAP2) are for general usage. Each of these map one to one to a TLB, where the calculation is:
There are no classes used for this range of virtIDs. An input virtID that is beyond the MAX_CNT bitfield value will produce an error.