SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
If a bus error is detected on a response to a ring memory transaction, an error event is triggered to alert software. Since the ring contents may be corrupted as the push or pop was not completed correctly, software should consider resetting the ring and any software or hardware elements using the ring. A log register (RINGACC_ERROR_LOG) captures the ring that had the error and whether it was from a push or pop, and an error up event is sent to the programmed event number. After an error is logged, another will not be captured until the first is read out. When read, if an error is pending an error down event is sent to clear any interrupt, and then the next bus error log can be captured. A read of the RINGACC_ERROR_LOG register when there is no error log pending will not produce any down events. The event that is triggered is also programmable. Only legal push and pop operations will capture this error, and not for any peek, emudbg read, flush command, or any operations that is illegal and causes the resulting memory access to be flushed.