SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The AXI master port of the PCIe core has an AXI2VBUSM bridge that is used for high speed data transfer during data read/write transactions originated by remote devices over the PCIe link. This bridge provides the protocol translation between the AXI master interface of the PCIe controller core and the VBUSM interface used in the device.