SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
If an end of line delimiter is received by the Rx (write) side of the UTC the EOL_ADV field in the TR application specific flags field is used to advance the appropriate indices of the TR to the next level. Each EOL that is received will cause the TR to advance to the next specified loop iteration breaking as many intermediate loops as are required.