SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Chromatic aberration, also known as “color fringing” or “purple fringing”, is a common optical problem that occurs in low quality lens when a lens is either unable to bring all wavelengths of color to the same focal plane (Longitudinal Chromatic aberration), and/or when wavelengths of color are focused at different positions in the focal plane (Lateral Chromatic aberration) .
Figure 6-39 shows one example of Chromatic Aberration referred as Lateral Chromatic Aberration (LCA). In this case, all colors are in focus in the same plane, but the foci are not placed along the optical axis. CAC Hardware accelerator performs Lateral Chromatic aberration correction is as part of VISS Pipe line.