SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
A rollover bit is maintained for each timer, such that when reprogrammed, it is the carry bit from the sum of the current time (counter) and the relative reprogramming value for that timer. This has the effect that any timer whose rollover bit is currently set to a 1 will not expire in the current epoch.
When the counter transitions from 0xFFFF FFFF to 0x0000 0000, the timer control module changes the rollover bit for all timers from a 1 to a 0. All timers that previously did not have the rollover bit set, will expire when they are next visited by the state machine, as their timeout value was for the previous epoch.
The overall effect is that the timers continue to expire as expected, regardless of when the counter rollover occurs relative to the state machine.