SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The MSMC has the following registers for interrupt control:
Each bit in these registers represents a single event or interrupt supported by MSMC, which generates only one interrupt. This is the null slave error interrupt (MSMC_NULL_SLAVE_ERROR). MSMC sets this event when routing a command through the MSMC null slave port which results in an unsuccessful response status. Commands failing firewall checks do not trigger the null slave error interrupt event in MSMC.