SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
In surround view use case, some regions of the frame won’t be used for stitching of final frame. By programming VPAC_LDC_REGION_CTRL_j[0] ENABLE to low, hardware will skip the processing of particular region.
Hardware has to make sure that FRAME_DONE information to LSE is generated on last pixel of last valid region.
As an example shown in Figure 6-94, Region-5, 7 and 8 are skipped for processing. FRAME_DONE is passed on last pixel of Region-6. Ordering and numbering of the regions will remain the same even in the case of skipping some regions.