SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
SPI legacy mode allows software to access the internal TX-FIFO and RX-FIFO directly, thus bypassing the direct, indirect and STIG controllers.
Legacy mode allows the user to issue any FLASH instruction to the device, but does place a heavy software overhead in order to manage the fill levels of the FIFO’s effectively. This is because the legacy SPI core is bi-directional in nature, with data continuously being transferred in either direction while the chip select is enabled. Even if the driver only wishes to read data from the FLASH device, dummy data must be written out to ensure the chip select stays active, and vice versa for write transactions.
Since the TX-FIFO and RX-FIFO are of limited depth, software has a responsibility to maintain the FIFO levels to ensure the TX-FIFO does not become exhausted during the instruction execution and the RX-FIFO doesn’t overflow. This can place a lot of overhead on software. Interrupts are provided to indicate when the fill levels pass programmable watermarks, which are themselves programmable registers OSPI_TX_THRESH_REG and OSPI_RX_THRESH_REG.
The limited depth may impose the limitation over execution of some specific SPI commands in legacy mode. Note that the controller interprets all transmitted bytes as valid. For example, if the Flash Device was configured to return valid data after many dummy cycles, the TX FIFO could become full before the controller sends all of dummy data.