SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The CSI_TX_IF controller uses a simple arbitration scheme for configurations with more than one pixel interface.
The arbitration has 2 levels; the first is a round-robin scheme and if no streams are granted by this a priority based scheme is used. The arbitration will select the first stream making a request if there is only one stream waiting or the first in the round robin after a stream has completed transmission. This means that there may be one cycle where the round-robin selector moves across a stream position that is not requesting to transmit.
The re-arbitration boundary is between packets except where line sync is used. In this case the line start packet, long packet and line end are grouped together.
The selected stream will pass the line data from the stream FIFO to the line control block for distribution to the active PPI lanes of the DPHY_TX.