SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The CSI_TX_IF will perform data type interleaving with one, two, or more pixel interfaces. In this scenario, Stream0 will be the master and one or more streams may be ganged together as slaves to the master stream. Therefore, for all the ganged streams, the virtual channel signals must be configured to the same value and the pixel streams must have the same active frame valid cycle (that is the virtual_channel_if* and frame_valid_if* must be wired in parallel). The STREAM_IF_*_SLAVE_MODE bit in the STREAM_IF_*_CFG registers must also be set for all slaved streams. This ensures that only one frame start and frame end are generated for all the ganged streams. Note that the pixel 0 interface is always the master and slave bits exist for the other streams, in the control registers, to determine if they are to operate in master or slave mode.
In the case where streams are ganged together as master and slave(s), all ganged interfaces must have the same virtual channel value, but the pixel_dt_sel_if inputs must be set to different values. Again, each of the interfaces can have the pixel_dt_sel_if input change on a line by line basis, so that interleaving is done with all the ganged streams.
Each stream must have exclusive use of the data types allocated to it.
Data type interleaving is only done when the frame is valid (CSI_TX_IF_DEBUG_PROT*_FSM[11] FRAME_VALID_IF* bitfield input is asserted). The virtual channel will be sampled on the first cycle after the rising edge of the FRAME_VALID_IF input and this virtual channel will be used for all the packets originating from that stream during that frame. The FRAME_VALID_IF input must be the same on all ganged stream interfaces.