SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The incoming data interface address, by default, maps directly to the address sent serially to the FLASH device. If the FLASH device has a 24-bit address, then the 24 LSB's of the data address is forwarded. A remap feature is available to remap all incoming data addresses to ADDRESS + N, where N is the value stored in the OSPI_REMAP_ADDR_REG[31-0] VALUE_FLD bit field. It is enabled via the OSPI_CONFIG_REG[16] ENB_AHB_ADDR_REMAP_FLD bit. This feature could be used when software needs to move boot code to another FLASH region.