SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
This is a very basic case, which does not need transferring statistics between cache memory and SDRAM. The most common example is video capture. In this case, the most straight forward way to run GLBCE, is to generate statistics from N-th frame, and apply it to (N+1)-th frame. The effect from using statistics of different frame should be small if the difference between frames is small. For example, it is expected this does not generate artifact, if the video frame rate is 30fps or larger. Below this rate, the single frame processing programming model explained in Section 6.7.3.5.7 should be considered.
In the case of continuous frame processing, GLBCE is operated in the following manner:
For the first frame of a set of sequential frames, Strength parameter should be 0, so GLBCE does not affect the image based on wrong statistics. SW may need to increase the strength value gradually after the first frame.