SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
FILE: dcc_ex2_single_shot_measurement.c
This program demonstrates Single Shot measurement of the SYSOSCDIV4 clock post trim using XTAL as the reference clock.
The Dual-Clock Comparator Module 0 is used for the clock measurement. The clocksource0 is the reference clock (Fclk0 = 20Mhz) and the clocksource1 is the clock (SYSOSCDIV4) that needs to be measured (Fclk1 = 8 hz). Since the frequency of the clock1 needs to be measured an initial seed is set to the max value of the counter.
Please refer to the TRM for details on counter seed values to be set.
External Connections