SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
The DMA contains overrun detection logic. When a peripheral event trigger is received by the DMA, the PERINTFLG bit in the CONTROL register is set, pending the channel to the DMA state machine. When the burst for that channel is started, the PERINTFLG is cleared. If however, between the time that the PERINTFLG bit is set by an event trigger and cleared by the start of the burst, an additional event trigger arrives, the second trigger is lost. This condition sets the OVRFLG bit in the CONTROL register as in Figure 10-7. If the overrun interrupt is enabled, the channel interrupt is generated to the PIE module.
Figure 10-7 Overrun
Detection Logic