SPRUJD3A July 2025 – October 2025 F28E120SB , F28E120SC
The UART provides a 9-bit mode that is enabled with the 9BITEN bit in the UART9BITADDR register. This feature is useful in a multi-drop configuration of the UART, where a single transmitter connected to multiple receivers can communicate with a particular receiver through the address or set of addresses along with a qualifier for an address byte. All the receivers check for the address qualifier in the place of the parity bit and, if set, then compare the byte received with the preprogrammed address. If the address matches, then the receiver receives or sends further data. If the address does not match, the receiver drops the address byte and any subsequent data bytes. If the UART is in 9-bit mode, then the receiver operates with no parity mode. The address can be predefined to match with the received byte and the address can be configured with the UART9BITADDR register. The matching can be extended to a set of addresses using the address mask in the UART9BITAMASK register. By default, the UART9BITAMASK is 0xFF, meaning that only the specified address is matched.
When not finding a match, the rest of the data bytes with the ninth bit cleared are dropped. If a match is found, then an interrupt is generated to the NVIC for further action. The subsequent data bytes with the cleared ninth bit are stored in the FIFO. Software can mask this interrupt in case DMA or FIFO operations are enabled for this instance and processor intervention is not required. All the send transactions with 9-bit mode are data bytes and the ninth bit is cleared. Software can override the ninth bit to be set (to indicate address) by overriding the parity settings to sticky parity with odd parity enabled for a particular byte. To match the transmission time with correct parity settings, the address byte can be transmitted as a single then a burst transfer. The transmit FIFO does not hold the address/data bit; hence, software can enable the address bit appropriately.